You are here: Introducing Kollmorgen Automation Suite > KAS breakdown

KAS Breakdown

Domains Concept (Technology) Task (Tools) Reference
HMI
  Kollmorgen Visualization Builder
Add an HMI
HMI
Controllers – PDMM & PCMM
Programmable Drive Multi-axis Master Add Controller
Configure Controller
Controller
Controllers – PAC
Industrial PC
Programmable Automation Controllers Add Controller
Configure Controller
Controller
PLC
PLC
IEC 61131-3 ST editor
IL editor
FBD editor
FFLD editor
SFC editor
 
Variable dictionary
Softscope
ST Language
IL Language
FBD Language
FFLD Language
SFC Language
Motion Engine
Motion
Motion Concept
Pipe Network
Design Pipe Network
Pipe Network Editor
Design CAM
Cam Profile Editor
Softscope
 
PLCopen
Operating System XP embedded
INtime
   
Fieldbus
Fieldbus
EtherCAT
Profibus"Process Field Bus" Profibus is the most popular type of fieldbus (see Fieldbus entry in the glossary) used worldwide
Configure EtherCAT Motion Bus Motion bus
Cables
I/O Terminal
I/O Modules
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs Add I/O terminal
I/O mapping to variable
I/O Editor
Remote Input/Output (I/O Terminals)

Drive
Drive

 
AKD
S300
S700
AKD-C
AKD-N
Add and configure drive
Drive Configuration
AKD Firmware Download
AKD
Motor
Motor
Kollmorgen Servomotor   AKM
Mechanical
Mechanical
    Linear Positioners
Gearheads

Table 2-3: KAS - Technologies and Tools

 

Human Machine Interface

PAC and Touch Panel PC

Programmable Drive Multi-Axis Master (AKD PDMM)

Operating System

Communication / Fieldbus

Machine for Input Output

Drive

Motor


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™